Part Number: DRV8312-C2-KIT
Other Parts Discussed in Thread: INSTASPIN-BLDC, CONTROLSUITE
Hello all,
I recently ordered a DRV8312-c2-kit for the purpose of comparing sensorless FOC and Trapezoidal motor control. The kit came with a flash drive containing the necessary applications (I think at least), as well as a manual, but when going through the manual I found that there was supposed to be another directory storing drivers for the F28035 piccolo control card. I would use these drivers to update the xds100 drivers (I think). When running the main application and trying to connect to the evaluation board I got a VCP auto-connection error.
All I'm missing is this directory. Where would I be able to find these files online?
For reference, the flash drive has the following:
GUI folder, containing DRV8312GUIv5.exe/.out and InstaSPIN-BLDC_GUI_DRV83xx_v104.exe/.out
controlsuiteinstaller.exe
As well as the two manuals (QSG-DRV8312-C2-KIT-GUI-InstaSPIN_BLDCv100.pdf and QSG-DRV8312-C2-KIT-GUIv1_1.pdf)
Thanks,
Scott