This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2812: power problems

Part Number: TMS320F2812


Pls review Our control Board schematic diagram:

I test total current about two DSP in our PCBA :

1.8V power, I_VDD(1.8V)+VDD1=359mA 

3.3V power, I_ VDDIO(3.3V)+VDDA1/2/IO=156mA

It seemed that the power have exceed the IDDIO(30mA*2)+IDDA(40mA*2)=140mA, if the margin is not enough for 3.3V and 1.8V power in my design, pls note I design a common power supply 1.8V for VDD1 and VDD, 3.3V for VDDA1/2/IO and VDDIO, could you give some suggestion about DSP power margin design?and give some risk about my design DSP running speed.