This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EPWM programming for simple boost control of single phase Z-source inverter(LAUNCHXL-F28069M)



Hi,

Lately I've been trying to program my F28069M launchpad for simple boost control of single phase Z-source inverter. I wish to get the switches in the same leg of inverter to be switched ON for 33microseconds in one complete cycle for 10kHz switching frequency. I have programmed some part of it but I am unable to program the 33microseconds overlap

// TI File $Revision: /main/2 $

//###########################################################################
//
// FILE: Example_2806xCpuTimer.c
//
// Description:
//
// This example configures CPU Timer0, 1, and 2 and increments
// a counter each time the timer asserts an interrupt.
//
// Watch Variables:
// CpuTimer0.InterruptCount
// CpuTimer1.InterruptCount
// CpuTimer2.InterruptCount
//
//###########################################################################

//###########################################################################

#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
#include <math.h>
#define RED_delay = 170;
#define FED_delay = 170;
// Prototype statements for functions found within this file.
interrupt void cpu_timer0_isr(void);
interrupt void cpu_timer1_isr(void);
interrupt void cpu_timer2_isr(void);
float t=0, w , w2 , pi=3.14159265,V;
int i=0,j=0;

float u[1000];
float ch1[334];

// Prototype statements for functions found within this file.
void InitEPwm1Example(void);
void InitEPwm2Example(void);
void InitEPwm3Example(void);

Uint16 EPwm_CMPA_Direction;
Uint16 EPwm_CMPB_Direction;
Uint16 EPwmTimerIntCount;
Uint16 EPwmMaxCMPA;
Uint16 EPwmMinCMPA;
Uint16 EPwmMaxCMPB;
Uint16 EPwmMinCMPB;

// Configure the period for each timer
#define EPWM1_TIMER_TBPRD 4000 // Period register
#define EPWM1_MAX_CMPA 1320
#define EPWM1_MIN_CMPA 50
#define EPWM1_MAX_CMPB 1320
#define EPWM1_MIN_CMPB 50

#define EPWM2_TIMER_TBPRD 4000 // Period register
#define EPWM2_MAX_CMPA 1320
#define EPWM2_MIN_CMPA 50
#define EPWM2_MAX_CMPB 1320
#define EPWM2_MIN_CMPB 50

#define EPWM3_TIMER_TBPRD 4000 // Period register
#define EPWM3_MAX_CMPA 1320
#define EPWM3_MIN_CMPA 50
#define EPWM3_MAX_CMPB 1320
#define EPWM3_MIN_CMPB 50

// To keep track of which way the compare value is moving
#define EPWM_CMP_UP 1
#define EPWM_CMP_DOWN 0

void main(void)
{
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2806x_SysCtrl.c file.
InitSysCtrl();

// Step 2. Initalize GPIO:
// This example function is found in the F2806x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio(); // Skipped for this example

EALLOW;
GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 0; // GPIO18 = GPIO18
GpioCtrlRegs.GPADIR.bit.GPIO18 = 1; // GPIO18 = output ->1

GpioCtrlRegs.GPAMUX2.bit.GPIO16 = 0; // 0=GPIO,
GpioCtrlRegs.GPADIR.bit.GPIO16 = 1; // 1=OUTput, 0=INput
GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 0; // 0=GPIO,
GpioCtrlRegs.GPADIR.bit.GPIO19 = 1; // 1=OUTput, 0=INput

GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0;
GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1;
GpioCtrlRegs.GPADIR.bit.GPIO0 = 1;
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // GPIO1 = epwm
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // GPIO1 = epwm
GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // GPIO1 = epwm
GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1; // GPIO1 = epwm
GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 1; // GPIO1 = epwm
GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 1; // GPIO1 = epwm

EDIS;
EALLOW;
SysCtrlRegs.PCLKCR0.bit.ADCENCLK = 1; // Enable ADC peripheral clock
(*Device_cal)(); // Auto-calibrate from TI OTP
SysCtrlRegs.PCLKCR0.bit.ADCENCLK = 0; // Return ADC clock to original state
EDIS;

// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;

// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2806x_PieCtrl.c file.
InitPieCtrl();

// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;

// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2806x_DefaultIsr.c.
// This function is found in F2806x_PieVect.c.
InitPieVectTable();

// For this example, only initialize the ePWM
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;

//Configure ADC
EALLOW;
SysCtrlRegs.PCLKCR0.bit.ADCENCLK = 1; // ADC
AdcRegs.ADCCTL1.bit.ADCREFSEL = 0; // Use internal bandgap
AdcRegs.ADCCTL1.bit.ADCBGPWD = 1; // Power up band gap
AdcRegs.ADCCTL1.bit.ADCREFPWD = 1; // Power up reference
AdcRegs.ADCCTL1.bit.ADCPWDN = 1; // Power up rest of ADC
AdcRegs.ADCCTL1.bit.ADCENABLE = 1; // Enable ADC
// for(i=0; i<5000; i++){} // wait 60000 cycles = 1ms (each iteration is 12 cycles)

AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1; // create int pulses 1 cycle prior to output latch

//set S/H window to 6 clk cycles (112.5ns)
AdcRegs.ADCSOC0CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC1CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC2CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC4CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC5CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC6CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC9CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC8CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC10CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC12CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC14CTL.bit.ACQPS = 8;


AdcRegs.INTSEL1N2.bit.INT1SEL = 12; // ADCCH12 (ADC-B4) EOC causes ADCInterrupt 1
AdcRegs.INTSEL1N2.bit.INT1CONT = 1; // set ADCInterrupt 1 to auto clr
AdcRegs.INTSEL1N2.bit.INT1E = 1; // enable ADC interrupt 1

//Note that SOC3, 7, 11, 13 & 15 are valid, but these SOCs are not configured
//since these ADC outputs do not exist on the controlSTICK. The configuration
//is configured as it is for readability.

//EOC = end of conversion event; SOC = start of conversion event
AdcRegs.ADCINTSOCSEL1.bit.SOC0 = 1; // ADCInterrupt 1 causes SOC0
AdcRegs.ADCINTSOCSEL1.bit.SOC1 = 1;
AdcRegs.ADCINTSOCSEL1.bit.SOC2 = 1;
AdcRegs.ADCINTSOCSEL1.bit.SOC4 = 1;
AdcRegs.ADCINTSOCSEL1.bit.SOC5 = 1;
AdcRegs.ADCINTSOCSEL1.bit.SOC6 = 1;
AdcRegs.ADCINTSOCSEL2.bit.SOC8 = 1;
AdcRegs.ADCINTSOCSEL2.bit.SOC9 = 1;
AdcRegs.ADCINTSOCSEL2.bit.SOC10 = 1;
AdcRegs.ADCINTSOCSEL2.bit.SOC12 = 1;
AdcRegs.ADCINTSOCSEL2.bit.SOC14 = 1;

//Select the channel to be converted when SOCx is received
AdcRegs.ADCSOC0CTL.bit.CHSEL= 0; // convert ADC-A0 (CH0) when SOC0 is received
AdcRegs.ADCSOC1CTL.bit.CHSEL= 1; // convert ADC-A1 (CH1) when SOC1 is received
AdcRegs.ADCSOC2CTL.bit.CHSEL= 2;
AdcRegs.ADCSOC4CTL.bit.CHSEL= 4;
AdcRegs.ADCSOC5CTL.bit.CHSEL= 5;
AdcRegs.ADCSOC6CTL.bit.CHSEL= 6;
AdcRegs.ADCSOC8CTL.bit.CHSEL= 8;
AdcRegs.ADCSOC9CTL.bit.CHSEL= 9; // convert ADC-B1 (CH9) when SOC9 is received
AdcRegs.ADCSOC10CTL.bit.CHSEL= 10;
AdcRegs.ADCSOC12CTL.bit.CHSEL= 12;
AdcRegs.ADCSOC14CTL.bit.CHSEL= 14;


EDIS;

AdcRegs.ADCSOCFRC1.all = 0x1000; // kick start ADC by causing a SOC12 event


InitEPwm1Example();
InitEPwm2Example();
InitEPwm3Example();

EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;

// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.TINT0 = &cpu_timer0_isr;
PieVectTable.TINT1 = &cpu_timer1_isr;
PieVectTable.TINT2 = &cpu_timer2_isr;
EDIS; // This is needed to disable write to EALLOW protected registers

// Step 4. Initialize the Device Peripheral. This function can be
// found in F2806x_CpuTimers.c
InitCpuTimers(); // For this example, only initialize the Cpu Timers

// Configure CPU-Timer 0, 1, and 2 to interrupt every second:
// 80MHz CPU Freq, 1 second Period (in uSeconds)

ConfigCpuTimer(&CpuTimer0, 80, 60);
ConfigCpuTimer(&CpuTimer1, 80, 1000000);
ConfigCpuTimer(&CpuTimer2, 80, 1000000);

// To ensure precise timing, use write-only instructions to write to the entire register. Therefore, if any
// of the configuration bits are changed in ConfigCpuTimer and InitCpuTimers (in F2806x_CpuTimers.h), the
// below settings must also be updated.

CpuTimer0Regs.TCR.all = 0x4001; // Use write-only instruction to set TSS bit = 0
CpuTimer1Regs.TCR.all = 0x4001; // Use write-only instruction to set TSS bit = 0
CpuTimer2Regs.TCR.all = 0x4001; // Use write-only instruction to set TSS bit = 0

// Step 5. User specific code, enable interrupts:


// Enable CPU int1 which is connected to CPU-Timer 0, CPU int13
// which is connected to CPU-Timer 1, and CPU int 14, which is connected
// to CPU-Timer 2:
IER |= M_INT1;
IER |= M_INT13;
IER |= M_INT14;

// Enable TINT0 in the PIE: Group 1 interrupt 7
PieCtrlRegs.PIEIER1.bit.INTx7 = 1;

// Enable global Interrupts and higher priority real-time debug events:
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM

/// default values
// Set the output relays on
GpioDataRegs.GPADAT.bit.GPIO19=1; //pin 25 relay1 to turn on
GpioDataRegs.GPADAT.bit.GPIO16=1; //pin 24 relay2 to turn on


// Step 6. IDLE loop. Just sit and loop forever (optional):
for(;;);

}


interrupt void cpu_timer0_isr(void)
{
CpuTimer0.InterruptCount++;
{
GpioDataRegs.GPADAT.bit.GPIO18 = 1; // for control loop timing
w= 2*pi*50;
//w2= 120* pi/ 180;

if(t>=100)
t=0;
t = t + 60e-6;

EPwm1Regs.CMPA.half.CMPA = (800*sin(w*t)+ 800) ;
EPwm1Regs.CMPB = (800*sin(w*t)+ 800) ;

EPwm2Regs.CMPA.half.CMPA =(800*sin(w*t)+ 800) ;
EPwm2Regs.CMPB =(800*sin(w*t)+ 800) ;

//EPwm3Regs.CMPA.half.CMPA =(1000*sin(w*t-(w2))+ 1000) ;
//EPwm3Regs.CMPB =(1000*sin(w*t-(w2))+ 1000) ;
V=(AdcResult.ADCRESULT0*3.3)/4095;

if(j>334)
j=0;
ch1[j]=V;
j=j+1;


GpioDataRegs.GPADAT.bit.GPIO18 = 0;

}

// Acknowledge this interrupt to receive more interrupts from group 1
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}

interrupt void cpu_timer1_isr(void)
{
CpuTimer1.InterruptCount++;
// The CPU acknowledges the interrupt.

}


interrupt void cpu_timer2_isr(void)
{ EALLOW;
CpuTimer2.InterruptCount++;

{
GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1; // Toggle GPIO34 once per cycle

}
EDIS;
// The CPU acknowledges the interrupt.


}


void InitEPwm1Example()
{

// Setup TBCLK
EPwm1Regs.TBPRD = EPWM1_TIMER_TBPRD; // Set timer period 801 TBCLKs
EPwm1Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm1Regs.TBCTR = 0x0000; // Clear counter

// Set Compare values
EPwm1Regs.CMPA.half.CMPA = EPWM1_MIN_CMPA; // Set compare A value
EPwm1Regs.CMPB = EPWM1_MAX_CMPB; // Set Compare B value

// Setup counter mode
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;

// Setup shadowing
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on Zero
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

// Set actions
EPwm1Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM1A on event A, up count
EPwm1Regs.AQCTLA.bit.CAD = AQ_CLEAR; // Clear PWM1A on event A, down count

EPwm1Regs.AQCTLB.bit.CBU = AQ_CLEAR; // Set PWM1B on event B, up count
EPwm1Regs.AQCTLB.bit.CBD = AQ_SET; // Clear PWM1B on event B, down count
EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; // enable Dead-band module
EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; // Active Hi complementary
//EPwm1Regs.DBFED = 170; // FED = 50 TBCLKs initially
//EPwm1Regs.DBRED = 170; // RED = 50 TBCLKs initially
}

void InitEPwm2Example()
{

// Setup TBCLK
EPwm2Regs.TBPRD = EPWM2_TIMER_TBPRD; // Set timer period 801 TBCLKs
EPwm2Regs.TBPHS.half.TBPHS = 0; // Phase is 0
EPwm2Regs.TBCTR = 0x0000; // Clear counter

// Set Compare values
EPwm2Regs.CMPA.half.CMPA = EPWM2_MIN_CMPA; // Set compare A value
EPwm2Regs.CMPB = EPWM2_MIN_CMPB; // Set Compare B value

// Setup counter mode
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;

// Setup shadowing
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on Zero
EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

// Set actions
EPwm2Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM1A on event A, up count
EPwm2Regs.AQCTLA.bit.CAD = AQ_CLEAR; // Clear PWM1A on event A, down count

EPwm2Regs.AQCTLB.bit.CBU = AQ_CLEAR; // Set PWM1B on event B, up count
EPwm2Regs.AQCTLB.bit.CBD = AQ_SET; // Clear PWM1B on event B, down count
EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; // enable Dead-band module
EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; // Active Hi complementary
//EPwm2Regs.DBFED = 170; // FED = 50 TBCLKs initially
//EPwm2Regs.DBRED = 170; // RED = 50 TBCLKs initially

EPwm2Regs.AQCTLB.bit.ZRO = 0; // Clear PWM2B on zero
EPwm2Regs.AQCTLB.bit.PRD = 1 ; // Set PWM2B on period


}

void InitEPwm3Example(void)
{
// Setup TBCLK
EPwm3Regs.TBPRD = EPWM3_TIMER_TBPRD; // Set timer period 801 TBCLKs
EPwm3Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm3Regs.TBCTR = 0x0000; // Clear counter

// Set Compare values
EPwm3Regs.CMPA.half.CMPA = EPWM3_MIN_CMPA; // Set compare A value
EPwm3Regs.CMPB = EPWM3_MIN_CMPB; // Set Compare B value

// Setup counter mode
EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm3Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV1;

// Setup shadowing
EPwm3Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm3Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm3Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on Zero
EPwm3Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

// Set actions
EPwm3Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM1A on event A, up count
EPwm3Regs.AQCTLA.bit.CAD = AQ_CLEAR; // Clear PWM1A on event A, down count

EPwm3Regs.AQCTLB.bit.CBU = AQ_CLEAR; // Set PWM1B on event B, up count
EPwm3Regs.AQCTLB.bit.CBD = AQ_SET; // Clear PWM1B on event B, down count
EPwm3Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; // enable Dead-band module
EPwm3Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; // Active Hi complementary
//EPwm3Regs.DBFED = 170; // FED = 50 TBCLKs initially
//EPwm3Regs.DBRED = 170; // RED = 50 TBCLKs initially

EPwm3Regs.AQCTLB.bit.ZRO = 0; // Clear PWM3B on zero
EPwm3Regs.AQCTLB.bit.PRD = 1 ; // Set PWM3B on period


}

What should I do? Am I programming it incorrectly? 

Thank you