Part Number: TMS320F28027F
Other Parts Discussed in Thread: DRV8305
Hello,
I am using a PMSM motor with the DRV8305.
Once the motor is identified I try to run lab 5b and when I do so, I am not able to get a smooth run from the motor.
Once in a while it will start turning smoothly, and as soon as I apply any load it will start to stall and overheat.
The motor reaches a very high temperature and I have to turn it off. I dont understand the issue with this motor.
What should i do to fix this problem ?
Regards,
Rajan Joshi