Other Parts Discussed in Thread: C2000WARE
Hello,
I am using comparator submodule to generate a trip, which is connected to ePWM tripzone. I have configured trip as one-shot. I see that OST flag is 1 in TZFLG but INT flag stays at 0. I need the interrupt to be generated so that I can set necessary variables in my ISR. Why interrupt is not getting generated?
Comparator and EPWM initialization.
EALLOW; /**** Step 1: Enable and configure Compare subsystem. ****/ //Enable CMPSS Cmpss3Regs.COMPCTL.bit.COMPDACE = 1; //NEG signal comes from DAC Cmpss3Regs.COMPCTL.bit.COMPHSOURCE = INTERNAL_DAC; //Use VDDA as the reference for DAC Cmpss3Regs.COMPDACCTL.bit.SELREF = REFERENCE_VDDA; //Set DAC to midpoint for arbitrary reference Cmpss3Regs.DACHVALS.bit.DACVAL = 1118; //Set to typical hysteresis Cmpss3Regs.COMPHYSCTL.bit.COMPHYS = TYPICAL_1x; /**** Step 2: Configure Digital Filter ****/ //Maximum CLKPRESCALE value provides the most time between samples Cmpss3Regs.CTRIPHFILCLKCTL.bit.CLKPRESCALE = 0; // 0 prescale => max resolution (10ns) //Maximum SAMPWIN value provides largest number of samples Cmpss3Regs.CTRIPHFILCTL.bit.SAMPWIN = 13; //Maximum THRESH value requires static value for entire window //THRESH should be GREATER than half of SAMPWIN Cmpss3Regs.CTRIPHFILCTL.bit.THRESH = 7; /**** Step 3: Initialize the sample values in the digital FIFO ****/ //Do not use initialization. On reset, all FIFO values would be zeros. Cmpss3Regs.CTRIPHFILCTL.bit.FILINIT = 0; /**** Step 4: Configure CTRIPOUT path ****/ //Digital filter output feeds CTRIPH and CTRIPOUTH Cmpss3Regs.COMPCTL.bit.CTRIPHSEL = CTRIP_FILTER; Cmpss3Regs.COMPCTL.bit.CTRIPOUTHSEL = CTRIP_FILTER; /**** Step 5: Configure ePWM X-bar modules to accept filter output ****/ //Configure TRIP5 to be CTRIP3H EPwmXbarRegs.TRIP5MUX0TO15CFG.bit.MUX4 = 0; //Enable TRIP5 Mux for Output EPwmXbarRegs.TRIP5MUXENABLE.bit.MUX4 = 1; /**** Step 6: Configure EPWM registers ****/ //Configure EPWM output A & B to go low on trip. EPwm2Regs.TZCTL.bit.TZA = TZ_FORCE_LO; EPwm2Regs.TZCTL.bit.TZB = TZ_FORCE_LO; //Configure DCA to be TRIP5 EPwm2Regs.TZDCSEL.bit.DCAEVT1 = TZ_DCBH_HI; EPwm2Regs.DCTRIPSEL.bit.DCAHCOMPSEL = 0x4; // Trip5 EPwm2Regs.DCAHTRIPSEL.bit.TRIPINPUT5 = 0; // Single trip input; Not ORed //Configure DCA as OST EPwm2Regs.TZSEL.bit.DCAEVT1 = 1; // Enable //Configure DCA path to be unfiltered & async EPwm2Regs.DCACTL.bit.EVT1SRCSEL = DC_EVT1; EPwm2Regs.DCACTL.bit.EVT1FRCSYNCSEL = DC_EVT_ASYNC; // Clear trip flags EPwm2Regs.TZCLR.bit.OST = 1; EPwm2Regs.TZCLR.bit.INT = 1; //Enable DCA interrupt EPwm2Regs.TZEINT.bit.OST = 1; EDIS;