This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: Some questions about how to use the CLA ?

Part Number: TMS320F28377S

Hi,all

I have two questions about F28377S CLA.

1.  When I run the countrolsuit  examples ,everything is OK. But when I imitate the examples , I will face the following questions. In the process of debugging the CLA, I connected CPU1 and CLA1 respectively. Load Program to CPU1 and load symbol to CLA1. Currently I  use CLA to complete a simple task, I just want to pass the value of "a" through CLA to "c", "a" and "c" are defined in CpuToCla1MsgRAM and Cla1ToCpuMsgRAM. When debugging, I can see the program can enter into Cla1Task1, But the CLA does not perform the assignment  in Cla1Task1. 

2.  When the CLA is working, can the CPU work at the same time? Are these two parallel relationships?

Thank you for your browsing and reply!!!