Part Number: TMDSSOLARUINVKIT
We are attempting to use these development kits to emulate PV generation in a smart grid. We started with the original build 3 and adjusted the AC voltage for our 26 volt emulated grid. We also disabled MPPT since we are using a DC power source for the inverter input. The board ran without issue with these two modifications. The third modification was to change the code so that the inverter board booted up in PVinverter active mode (the idea was to have the boards run without having to be flashed/initialized each time they are power cycled). The first time we ran the code it booted up and operated without issue. The second time the controls were not responsive and we observed that even with the controller off the board draws current from the source indicating a possible short. I examined the board and was unable to see any visible damage. I have tried using pervious versions of the code with no impact. I would appreciate any support you can provide.