Part Number: TMS320F28075
Hello,
I have a GPIO configured as input to the tripzone. I also have input qualification 6 samples at SYSCLKOUT of 10ns. The configuration is as follows:
EALLOW; GpioCtrlRegs.GPAINV.bit.GPIO31 = 1; /* TZ active low - Input inversion control for this pin */ GpioCtrlRegs.GPACTRL.bit.QUALPRD3 = 0; /* Qual period = SYSCLKOUT = 10ns */ GpioCtrlRegs.GPAQSEL2.bit.GPIO31 = 2; /* Qual Samples = 6; Total samples=10 and if input is high for 6 samples (6*10ns=60ns), then it is REALLY high. */ GpioCtrlRegs.GPAPUD.bit.GPIO31 = 1; /* Enable pull-up on GPIO (TZx) - 1: Disables the Pull-Up. */ InputXbarRegs.INPUT1SELECT = 31; /* INPUT1 is link with TZ1 - PFC_TRIP */ EDIS;
My understanding is that if a signal is to be detected as actual input, it has to be high for 6 continuous samples. My question is that if it detect first 3 samples as high and next three as low, will the count start from 0 or from 4 for next sampling window?
In my system, one the input is high, I shut down the system. In the following oscilloscope picture, I see 6 high samples before shutting down but the timing is totally different (in terms of ms). It gives me an impression that it does not reset the counter value or something which is being used to check continuous 6 samples for high.
What am I missing?