Hi all,
Has anyone used the epwm Immediate Load Mode in f2808, I recently used it to generate a pwm signal with 50% duty cycle and frequency of 20KHz, the duty cycle is updated every 2.5us, but once in a while, the duty cycle changed to 100% which cannot be explained. This problem does not appear in shadow mode
Is there any examples from ti teaching how to use this mode?
What is the consequence if I use the Immediate Load Mode instead of the shadow mode to update the epwm?
Thanks!