This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28333: McBSP to Audio Codec PCM 3010

Part Number: TMS320F28333

Hey all, 

Im trying to interface an audio codec over Mcbsp however I have gone through settings many times and can not alter the frame sync period and width to obtain the proper LR clock. Thanks, I will attach some oscilloscope images.

/*
 * i2s.c
 *
 *  Created on: Jul 19, 2017
 *      Author: Ish's Master Race PC
 */
#include <DSP28x_Project.h>
#include <DSP2833x_Mcbsp.h>
#include "timer.h"


Uint32 sample_L = 0b10101010101010101010101010101010;
Uint32 sample_R = 0xFFFF;
Uint16 johns = 0xFFFF;
Uint16 johns2 = 0x7777;
int ch_sel = 0;

__interrupt void Mcbsp_TxINTA_ISR(void);
__interrupt void Mcbsp_RxINTA_ISR(void);

void InitMcbspaI2S(void);

void main(){
    DisableDog();
    InitPll(10,2);
    InitPeripheralClocks();
    InitMcbspaGpio();
    DINT;

        //
        // Initialize PIE control registers to their default state.
        // The default state is all PIE interrupts disabled and flags
        // are cleared.
        // This function is found in the DSP2833x_PieCtrl.c file.
        //
        InitPieCtrl();

        //
        // Disable CPU interrupts and clear all CPU interrupt flags
        //
        IER = 0x0000;
        IFR = 0x0000;

        //
        // Initialize the PIE vector table with pointers to the shell Interrupt
        // Service Routines (ISR).
        // This will populate the entire table, even if the interrupt
        // is not used in this example.  This is useful for debug purposes.
        // The shell ISR routines are found in DSP2833x_DefaultIsr.c.
        // This function is found in DSP2833x_PieVect.c.
        //
        InitPieVectTable();

        //
        // Interrupts that are used in this example are re-mapped to
        // ISR functions found within this file.
        //
        EALLOW;	                // Allow access to EALLOW protected registers
        PieVectTable.MRINTA= &Mcbsp_RxINTA_ISR;
        PieVectTable.MXINTA= &Mcbsp_TxINTA_ISR;
        EDIS;                   // Disable access to EALLOW protected registers

        //
        // Step 4. Initialize all the Device Peripherals:
        // This function is found in DSP2833x_InitPeripherals.c
        //
        // InitPeripherals(); // Not required for this example

        //
        // Enable interrupts required for this example
        //
        PieCtrlRegs.PIECTRL.bit.ENPIE = 1;      // Enable the PIE block
        PieCtrlRegs.PIEIER6.bit.INTx5=1;        // Enable PIE Group 6, INT 5
        PieCtrlRegs.PIEIER6.bit.INTx6=1;        // Enable PIE Group 6, INT 6
        // change when put in MAIN
        IER=0x20;                               // Enable CPU INT6
        EINT;                                   // Enable Global Interrupts
    InitMcbspaI2S();
    //timer_init(150.0,22.6757);
    //enable_timer_interrupt_DFT();
    //GpioCtrlRegs.GPAMUX2.bit.GPIO23 = 0; // demphasis 0
    GpioCtrlRegs.GPAMUX2.bit.GPIO24 = 0; // demphasis 0
    GpioCtrlRegs.GPAMUX2.bit.GPIO25 = 0; // demphasis 1
    GpioCtrlRegs.GPAMUX2.bit.GPIO26 = 0; // pdwn
    GpioDataRegs.GPADAT.bit.GPIO24 = 0;
    GpioDataRegs.GPADAT.bit.GPIO25 = 0;
    GpioDataRegs.GPADAT.bit.GPIO26 = 1;
    while(McbspaRegs.SPCR2.bit.XRDY == 0)
            McbspaRegs.DXR2.all = johns;
            McbspaRegs.DXR1.all = johns2;
    while(1) {
//    	while(McbspaRegs.SPCR2.bit.XRDY == 0)
//        McbspaRegs.DXR2.all = johns;
//        McbspaRegs.DXR1.all = johns2;
    }
}

void InitMcbspaI2S(void){
    /*
     * Connections
     * MCLKXA <- BCLK from DAC for transmit clock
     * MFSXA <- WCLK from DAC for frame sync signal
     */

	//Bit Clock set up
    		//word size * fs * 2 = 24 * 44100 * 2 = 2,116,800
    //Word Clock set up
    		//fs

// XCLKOUT SETUP
	EALLOW;
    SysCtrlRegs.PCLKCR0.bit.MCBSPAENCLK = 1;
    SysCtrlRegs.PCLKCR3.bit.XINTFENCLK = 1; //Enable external clock
    XintfRegs.XINTCNF2.bit.XTIMCLK = 1; //XCLKOUT is SYSCLKOUT/4
    XintfRegs.XINTCNF2.bit.CLKMODE = 1;//This makes for a 37.5MHz DAC MCLK
    XintfRegs.XINTCNF2.bit.CLKOFF = 0;
    EDIS;


// RESETTING ALL REGISTERS
	EALLOW;
	McbspaRegs.SPCR2.all=0x0000;// Reset FS generator, sample rate generator & transmitter
	McbspaRegs.SPCR1.all=0x0000; // Reset Receiver, Right justify word
	McbspaRegs.SPCR1.bit.RJUST = 2; // left-justify word in DRR and zero-fill LSBs
	McbspaRegs.MFFINT.all=0x0; // Disable all interrupts
	McbspaRegs.SPCR1.bit.RINTM = 0; // McBSP interrupt flag - RRDY, data ready to read
	McbspaRegs.SPCR2.bit.XINTM = 0; // McBSP interrupt flag - XRDY, data ready to accept new transfer
	McbspaRegs.RCR2.all=0x0; // Clear Receive Control Registers
	McbspaRegs.RCR1.all=0x0;
	McbspaRegs.XCR2.all=0x0; // Clear Transmit Control Registers
	McbspaRegs.XCR1.all=0x0;
	McbspaRegs.PCR.all=0x0000;

	//added stuffs
	McbspaRegs.SPCR1.bit.RINTM = 2;
	McbspaRegs.SPCR2.bit.XINTM = 2;
	McbspaRegs.SPCR2.bit.FREE = 1;
	McbspaRegs.RCR2.bit.RFIG = 0;
	McbspaRegs.XCR2.bit.XFIG = 0;


// CLOCKING
	//Source Clock
	McbspaRegs.PCR.bit.SCLKME = 0; //Sample rate from LSPCLK
	McbspaRegs.SRGR2.bit.CLKSM = 1; // LSPCLK is clock source for SRG
	McbspaRegs.SRGR1.bit.CLKGDV = 60; //Dividing down the LSPCLK
	McbspaRegs.PCR.bit.CLKXM = 1; // Internal transmit clock
	McbspaRegs.PCR.bit.CLKRM = 1; // Internal receive clock
	McbspbRegs.SRGR2.bit.FSGM = 1; //Frame synch pulses generated by sample rate generator
	McbspaRegs.PCR.bit.FSXM = 1; //Receive Frame sync is supplied by sample rate gen
	McbspaRegs.PCR.bit.FSRM = 1; //Transfer Frame sync is supplied by sample rate gen

    //TX, RX CLOCKS EDGES
	McbspaRegs.PCR.bit.CLKRP = 0; // Rcvd data sampled on rising edge of CLKR
	McbspaRegs.PCR.bit.CLKXP = 1; // Tx data sampled on falling edge of CLKX
	//FS Clock Edge
	McbspaRegs.PCR.bit.FSRP = 1; // Receive Frame synch pulse is active high (R-channel first)
	McbspaRegs.PCR.bit.FSXP = 1; // Transmit Frame synch pulse is active high (R-channel first)


// FRAME SYNC WIDTHS
    //Frame Sync Width
    McbspaRegs.SRGR2.bit.FPER = 47; //Period is 47 + 1
    McbspaRegs.SRGR1.bit.FWID = 23; //Pulse width is 23 + 1

    // 2 Receive phases, each is 1 word (24 bits)
    McbspaRegs.RCR1.bit.RWDLEN1 = 4; // receive word 1 is 24 bit data
	McbspaRegs.RCR1.bit.RFRLEN1 = 1; //receive frame length 1: 1 word
    McbspaRegs.RCR2.bit.RWDLEN2 = 4; // receive word 2 is 24 bit data
    McbspaRegs.RCR2.bit.RFRLEN2 = 1; //receive frame length 2: 1 word
    McbspaRegs.RCR2.bit.RPHASE =  0; //2 receive phase (left and right)
    // Data delays
	McbspaRegs.RCR2.bit.RDATDLY = 1;//length of data delay for receive (1 bit)

    // 2 Transfer phases, each is 1 word (24 bits)
    McbspaRegs.XCR1.bit.XWDLEN1 = 4; // tx word 1 is 24 bits
    McbspaRegs.XCR1.bit.XFRLEN1 = 1;//transfer frame length 2: 1 word
    McbspaRegs.XCR2.bit.XWDLEN2 = 4; // transmit 24 bit data
    McbspaRegs.XCR2.bit.XFRLEN2 = 1;//transfer frame length 2: 1 word
    McbspaRegs.XCR2.bit.XPHASE = 0;//2 transfer phase (left and right?)
    //Data Delay
	McbspaRegs.XCR2.bit.XDATDLY = 1;//length of data delay for transfer (1 bit)


// ENABLING
    //delay_loop();
    McbspaRegs.MFFINT.bit.XINT = 1; // Enable Transmit Interrupt
    McbspaRegs.MFFINT.bit.RINT = 1;
	delay_loop();
    McbspaRegs.SPCR2.bit.GRST   = 1;
    delay_loop();
    McbspaRegs.SPCR2.bit.XRST   = 1;
    McbspaRegs.SPCR1.bit.RRST   = 1;
    delay_loop();                      // need to wait at least 2*(1/100mHz)
    McbspaRegs.SPCR2.bit.FRST = 1;
    delay_loop();
    EDIS;
}

__interrupt void Mcbsp_TxINTA_ISR(void){
    if(0 == ch_sel){
        ch_sel = 1;
        McbspaRegs.DXR2.all = sample_L;
        McbspaRegs.DXR1.all = sample_L;
    }
    else{
        ch_sel = 0;
        McbspaRegs.DXR2.all = sample_R;
        McbspaRegs.DXR1.all = sample_R;
    }
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP6;
}

__interrupt void Mcbsp_RxINTA_ISR(void){

    PieCtrlRegs.PIEACK.all = PIEACK_GROUP6;
}

  • Hello Ishmael,

    Can you annotate your scope capture and share a little bit more? is the Blue signal your FSX? Yellow is MCLKX?
    Please set XPHASE to 1 since you are using a dual phase transmission, one for the left channel, one for the right channel.

    Please check out SPRA595 for an overview of using McBSP as I2S. IT is for the C6000 product line, but the McBSP module is equivalent, so the configurations will still be valid.

    Thanks,
    Mark