This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377S: GPIO clamp protection

Part Number: TMS320F28377S

Tool/software: Code Composer Studio

 I didn't find the clamp protection in GPIO of F2837x. So I think there is no clamp protection in GPIO. However, the C2000 MCU can work normally with 5V input because of my carelessness. 

So, there is a clamp protection in GPIO but no statement in datasheet, or there is no clamp protection.

  • Hello,
    I am writing to let you know that a C2000 team member has been assigned to this post and should be answering shortly.

    Regards
    Baskaran
  • and the value of the GPIO pull-up resistor is 10k? the default pullup set is disable? and the default GPIO output is high ?
  • Hi Houjian,

    The GPIOs will indeed begin clamping if an input is applied that is about 0.3V below VSS or about 0.3V above VDDIO.

    In order to avoid damaging the device, this clamping current should be limited to less than 20mA on a given pin and less than 20mA total for all pins at any time.  It is usually also best to avoid a situation where the pin is being continuously clamped (vs. a short transient clamping event).

  • We don't directly specify the pull up/down resistance, but you can find the pull currents in the datasheet table "5.6 Electrical Characteristics".

    There are pull-ups on all GPIO pins and they are disabled by default per section 4.2 Signal Descriptions: "All GPIO pins are I/O/Z and have an internal pullup, which can be selectively enabled or disabled on a per-pin basis. This feature only applies to the GPIO pins. The pullups are not enabled at reset." If you look at the TRM you can also see that the pull-up disable registers (e.g. GPAPUD) are disabled by default based on the reset value of the register.