Hi!
The description in spruhm8f.pdf(1070 page), the 5 bite of XBARFLG2 register is INPUT7, As shown in the below figure.
But after i test the inputxbar(i set one signal to the inputxbar.input6,then change the signal the xbarflags.input7 changed), in fact this bit is really is input6. The same as the XBARCLR2 register. Please confirm this information.thanks!
regards
shook