This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: Do I need to use MOSFET drive IC when using C2000?

Part Number: TMS320F28335


Hello

I am using the GPIO of the MCU as the gate voltage of the MOSFET. The GPIO is 3.3 V and the minimum threshold voltage of my MOSFET is 2.5 V and the drain voltage is 30 V. Do I need to use the MOSFET gate drive IC or can I connect the GPIO directly to gate of the MOSFET?

Best,

Ata