Part Number: TMS320F28052F
Other Parts Discussed in Thread: UNIFLASH
I am having a really strange issue across multiple programmers. I have two Elpotronics programmers, FlashPro2000 and C2000 Gang, and both of them can write to blank devices and then erase what they wrote and write it again, but if i power cycle the device so that it is running the code suddenly both throw out errors during the flash erase step. The strange thing is that i can come in with the XDS100v2 using Uniflash and erase the memory just fine and since its blank the other two programmers once again work fine on it.
This is a real issue cause I need one of the two other programmers to work, I have contacted Elpotronics but they don't seem to know what the problem is either. So what doe sthe XDS100v2 do that these other two don't?