This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28335: error #18: expected a ")", cannot find the root cause for this...

Part Number: TMS320F28335


Tool/software: Code Composer Studio

Hi,

I am experiencing a fault during the code compiling. The error code is: 

>> Compilation failure
subdir_rules.mk:184: recipe for target 'VehCtrl_Process.obj' failed
"..\DSP2833x_Adc.h", line 99: error #18: expected a ")"
Uint16 RESET:1; // 14 ADC reset

I was not able to target the error since the project is a little bit too large...

I attached a zip file which includes all the .pp file that generated. Can anyone help me figure out where the error comes from?

Thank you very much!

EXP9.zip