This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28PLC83: sci_echoback example for TMDSPLCKITV4-CEN

Part Number: TMS320F28PLC83


Tool/software: Code Composer Studio

Hello

I would like to set up the settings described in sci_echoback (controlSUITE\device_support\f2806x\v151\F2806x_examples\sci_echoback) but the example is suitable for TMDSPLCKIT-V3. It communicates by HyperTerminal with serial DB9 which my board (TMDSPLCKITV4-CEN) does not have.

Any suggestion, so I can execute the example?

Thank you

Luiz Bueno

  • Hi Luiz,

    I believe you should be able to run sci_echoback, if you connect the PLC docking station's J3 to your computer.

    Computer <-> USB cable <-> FTDI chip (performs USB-to-SCI conversion, among other things) <-> SOM connector <-> SCI-A (GPIO28/29) on the C2000 device


    Thanks,
    Brett