Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM
Hi TI,
I've accidently burned out my LAUNCHXL-F28379D board ver.1.1 in high voltage application using with BOOSTXL-DRV8305EVM and 430BOOST-SHARP96. The booster pack works well but the C2000 chip now has ultra-low impedance on 3.3V bus and became hot and unfunctional. And now I have programed my 50Hz inverter application using MSP430, but high frequency distortion is still in inappropriate level due to relatively low bus clock speed. Can I order patched version of LAUNCHXL-F28379D board without PIN#29 (ADCINA2) issue?
Regards,
Alexey