This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377D: Unable to debug the program: Error with TI XDS100 V2 driver

Part Number: TMS320F28377D

Tool/software: Code Composer Studio

Untill few days earlier i was using Windows 10 to run CCS v7, and it was working fine. Recently i had to change the OS and now I am using a fresh copy of Windows 7 Ultimate SP1. I have downloaded CCS v7 on windows 7, and since then I am unable to debug the program (builds successfully). I am attaching a screenshot below for the installed software from TI.

Do I need to Install some softwares for this to work? I didnt notice the softwares installed in windows 10 earlier. Kindly suggest some resolution.

--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

Also I have noticed 2 Texas Instrument's Devices being corrupt (i guess) in device manager. I am attaching the screenshot of this as well for anyone to refer.

Kindly suggest what & how to do? 

--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

There was a warning regarding a windows update while installation. Does that make any difference? 

I assume it is a security update so I don't think it can cause this.