Other Parts Discussed in Thread: MOTORWARE
Tool/software: Code Composer Studio
Hello,
I am working with LAUNCHXL-F28069M we are using our own inverter, voltage sensing(ACPL-C87A) & current sensing (LEM HASS-300S) my task for now was to run Torque control on our Axial Fux BLDC Motor. Which has been accomplished and tested thanks to this post.
But now when i am running the motor using lab11a with torque control their is noise issue. As the speed of the motor reaches close to rated speed (i.e. 2500rpm) then some noise starts to come from motor as if the poles are getting skipped. And when I test the motor with same Kp/Ki values with lab5a then their is no issue of noise and motor runs fine (Tested till 2800rpm). As lab11a don't have CTRL and has Field weakening & Overmodulation feature which are also been required for further tests i am obligated to use lab11a.
In this post