Other Parts Discussed in Thread: C2000WARE
Is there any jumper setting or a pin to be enabled to use the SCI A com port in the launchpad for f28379d ?
I am using the ft232 inbuilt
I am using the attached simulink model
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any jumper setting or a pin to be enabled to use the SCI A com port in the launchpad for f28379d ?
I am using the ft232 inbuilt
I am using the attached simulink model
now i installed c2000ware and using ccsv6
Out of box demo also not working for echo back , if a character is sent from the teminal, red LED, Rx for the corresponding serial in the board is lighting up, but the same not happening for blue led of serial Tx , if we communicate by terminal.
what can be the reason for not working ?, i have tried with 42 43 and 28 29 pins for sci
initially my file was not attaching, now got success with attaching
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/171/4544.untitled.7z
yes, got resolved here
e2e.ti.com/.../618663
Thanks for the support, since i have used a lot of threads, forgot to update in all