This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: TMS320F28035 Clock speed change in running

Part Number: TMS320F28035
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE

Dear all,

In my application using F28035, I should be manage current consumption as following.

- In measure mode using 7 ADC channels : 40mA max.

- In run mode : there is no limit.

I already checked Idle / Standby / Halt mode and FLASH OFF in F28035, but I did't get suite result.

So, I thought a changing clock speed at each mode in running as following.

- In measure mode using 7 ADC channels : 10MHz

- In run mode : 60MHz

Is it possible changing clock speed in running??

Dear Eui-heon