This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28062: Working of XCLKOUT

Part Number: TMS320F28062

Hello,

I want to ask about GPIO18/SPICLKA/SCITXDB/XCLKOUT (Pin No.51 in TMS320F28062 100-Pin PZ). 

Questions:

1. Will XCLKOUT give frequency with the use of Internal oscillator? Is there any need to apply frequency at XIN to get desired frequency out from XCLKOUT? 

2. What will the voltage level of that signal from XCLKOUT?

Thanks in advance.

Best regards,

Dinesh Jinjala 

  • Hi Dinesh,

    Dinesh P Jinjala said:
    1. Will XCLKOUT give frequency with the use of Internal oscillator? Is there any need to apply frequency at XIN to get desired frequency out from XCLKOUT? 

    XCLKOUT gives you the System clock or division of the same as per XCLKOUTDIV. System clock can be based out of internal or external oscillator/crystal.

    Dinesh P Jinjala said:
    2. What will the voltage level of that signal from XCLKOUT?

    Same as other GPIOs 3.3v

    Regards,

    Gautam