Hello all
I need some help
Can the C2000 generate two different signals,, the base frequency around 200khz to 300khz and the second at 11 times the base frequency?
or is their a better EVM for this task?
the base frequency needs to be adjustable between 200khz and 300khz.
or will I need a separate signal generator for the base frequency?
how can I access the library?
Thanks Jeff/Frosty