This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDXIDDK379D: DesignDrive queries

Part Number: TMDXIDDK379D
Other Parts Discussed in Thread: DESIGNDRIVE, CONTROLSUITE

Hello,

I had a few queries about the design drive.

  1. Do I get to choose the MCU among the ones in TMS320F287xx when I buy the product?
  2. Is it possible to provide the DC supply directly to the board?
  3. Can this evaluation be used to drive a DC motor? I understand that it can be used for sensored control of BLDC motor.
  4. Is UART or debug port available?
  5. What is used, CAN or EtherCAT?
  6. Is the communication protocol, RS422 or RS485?

I understand that most of these could be found out from data sheets. I need the data very soon. Please excuse the obviousness.