This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28035: c2000 CLA sqrt sample not working

Part Number: TMS320F28035
Other Parts Discussed in Thread: CONTROLSUITE

Tool/software: Code Composer Studio

C:\ti\controlSUITE\device_support\f2803x\v130\DSP2803x_examples_cla_ccsv5\sqrt

in above sample code for cla When I try to calculate sqrt of except other than 2 sample code  not working. I'm using Code Composer Studio Version: 7.2.0.0001. 

void test_run(void)

{

fVal = 2;                               
Cla1ForceTask1andWait();

#if 0
Cla1ForceTask2andWait();

Cla1ForceTask3andWait();

Cla1ForceTask4andWait();

Cla1ForceTask5andWait();

Cla1ForceTask6andWait();

Cla1ForceTask7andWait();

Cla1ForceTask8andWait();
#endif
}

void test_report(void)
{


if(fResult < 1.4143 && fResult > 1.4141)
puts("PASS\n");
else
printf("FAIL , fResult = %f\n",fResult);
}

  • lokks like printf routine stuck why ????????????
  • /*
    //###########################################################################
    //
    // FILE: F28035_CLA_C.cmd
    //
    // TITLE: Linker Command File For F28035 Device
    //
    //###########################################################################
    // $TI Release: F2803x C/C++ Header Files and Peripheral Examples V130 $
    // $Release Date: May 8, 2015 $
    // $Copyright: Copyright (C) 2009-2015 Texas Instruments Incorporated -
    // http://www.ti.com/ ALL RIGHTS RESERVED $
    //###########################################################################
    */

    /* ======================================================
    // For Code Composer Studio V2.2 and later
    // ---------------------------------------
    // In addition to this memory linker command file,
    // add the header linker command file directly to the project.
    // The header linker command file is required to link the
    // peripheral structures to the proper locations within
    // the memory map.
    //
    // The header linker files are found in <base>\DSP2803x_Headers\cmd
    //
    // For BIOS applications add: DSP2803x_Headers_BIOS.cmd
    // For nonBIOS applications add: DSP2803x_Headers_nonBIOS.cmd
    ========================================================= */

    /* ======================================================
    // For Code Composer Studio prior to V2.2
    // --------------------------------------
    // 1) Use one of the following -l statements to include the
    // header linker command file in the project. The header linker
    // file is required to link the peripheral structures to the proper
    // locations within the memory map */

    /* Uncomment this line to include file only for non-BIOS applications */
    /* -l DSP2803x_Headers_nonBIOS.cmd */

    /* Uncomment this line to include file only for BIOS applications */
    /* -l DSP2803x_Headers_BIOS.cmd */

    /* 2) In your project add the path to <base>\DSP2803x_headers\cmd to the
    library search path under project->build options, linker tab,
    library search path (-i).
    /*========================================================= */

    /* Define the memory block start/length for the F28035
    PAGE 0 will be used to organize program sections
    PAGE 1 will be used to organize data sections

    Notes:
    Memory blocks on F2803x are uniform (ie same
    physical memory) in both PAGE 0 and PAGE 1.
    That is the same memory region should not be
    defined for both PAGE 0 and PAGE 1.
    Doing so will result in corruption of program
    and/or data.

    L0 memory block is mirrored - that is
    it can be accessed in high memory or low memory.
    For simplicity only one instance is used in this
    linker file.

    Contiguous SARAM memory blocks or flash sectors can be
    be combined if required to create a larger memory block.
    */
    _Cla1Prog_Start = _Cla1funcsRunStart;
    -heap 0x200
    -stack 0x200

    // Define a size for the CLA scratchpad area that will be used
    // by the CLA compiler for local symbols and temps
    // Also force references to the special symbols that mark the
    // scratchpad are.
    // CLA_SCRATCHPAD_SIZE = 0x100;
    --undef_sym=__cla_scratchpad_end
    --undef_sym=__cla_scratchpad_start

    MEMORY
    {
    PAGE 0: /* Program Memory */
    /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
    RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
    RAML3 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L3 */
    OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
    FLASHH : origin = 0x3E8000, length = 0x002000 /* on-chip FLASH */
    FLASHG : origin = 0x3EA000, length = 0x002000 /* on-chip FLASH */
    FLASHF : origin = 0x3EC000, length = 0x002000 /* on-chip FLASH */
    FLASHE : origin = 0x3EE000, length = 0x002000 /* on-chip FLASH */
    FLASHD : origin = 0x3F0000, length = 0x002000 /* on-chip FLASH */
    FLASHC : origin = 0x3F2000, length = 0x002000 /* on-chip FLASH */
    FLASHA : origin = 0x3F6000, length = 0x001F80 /* on-chip FLASH */
    CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
    BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
    CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */

    IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */
    IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */
    IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */

    ROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */
    RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
    VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */

    PAGE 1 : /* Data Memory */
    /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
    /* Registers remain on PAGE1 */
    BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
    RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
    RAML0 : origin = 0x008000, length = 0x000800 /* on-chip RAM block L0 */
    CLARAM0 : origin = 0x008800, length = 0x000400
    CLARAM1 : origin = 0x008C00, length = 0x000400

    CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
    CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080

    FLASHB : origin = 0x3F4000, length = 0x002000 /* on-chip FLASH */

    }

    /* Allocate sections to memory blocks.
    Note:
    codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
    execution when booting to flash
    ramfuncs user defined section to store functions that will be copied from Flash into RAM
    */

    SECTIONS
    {

    /* Allocate program areas: */
    .cinit : > FLASHA PAGE = 0
    .pinit : > FLASHA, PAGE = 0
    .text : >> FLASHC | FLASHE PAGE = 0
    codestart : > BEGIN PAGE = 0
    ramfuncs : LOAD = FLASHD,
    RUN = RAMM0,
    LOAD_START(_RamfuncsLoadStart),
    LOAD_SIZE(_RamfuncsLoadSize),
    RUN_START(_RamfuncsRunStart),
    PAGE = 0

    csmpasswds : > CSM_PWL_P0 PAGE = 0
    csm_rsvd : > CSM_RSVD PAGE = 0

    /* Allocate uninitalized data sections: */
    .stack : > RAMM1 PAGE = 1
    .cio : >> RAML0 | RAMM1 PAGE = 1
    .sysmem : > RAMM1 PAGE = 1
    .ebss : > RAML0 PAGE = 1
    .esysmem : > RAML0 PAGE = 1


    /* Initalized sections go in Flash */
    /* For SDFlash to program these, they must be allocated to page 0 */
    .econst : > FLASHA PAGE = 0
    .switch : > FLASHA PAGE = 0

    /* Allocate IQ math areas: */
    IQmath : > FLASHA PAGE = 0 /* Math Code */
    IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD

    .bss_cla : > CLARAM0, PAGE = 1
    .scratchpad : > CLARAM0, PAGE = 1

    Cla1Prog : LOAD = FLASHD,
    RUN = RAML3,
    LOAD_START(_Cla1funcsLoadStart),
    LOAD_END(_Cla1funcsLoadEnd),
    RUN_START(_Cla1funcsRunStart),
    LOAD_SIZE(_Cla1funcsLoadSize),
    PAGE = 0

    Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
    CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1
    Cla1DataRam0 : > CLARAM0, PAGE = 1
    Cla1DataRam1 : > CLARAM1, PAGE = 1

    GROUP : LOAD = FLASHB,
    RUN = CLARAM1,
    LOAD_START(_Cla1mathTablesLoadStart),
    LOAD_END(_Cla1mathTablesLoadEnd),
    RUN_START(_Cla1mathTablesRunStart),
    LOAD_SIZE(_Cla1mathTablesLoadSize),
    PAGE = 1

    {
    CLA1mathTables
    .const_cla
    }

    CLAscratch :
    { *.obj(CLAscratch)
    . += CLA_SCRATCHPAD_SIZE;
    *.obj(CLAscratch_end) } > CLARAM0,
    PAGE = 1

    /* Uncomment the section below if calling the IQNexp() or IQexp()
    functions from the IQMath.lib library in order to utilize the
    relevant IQ Math table in Boot ROM (This saves space and Boot ROM
    is 1 wait-state). If this section is not uncommented, IQmathTables2
    will be loaded into other memory (SARAM, Flash, etc.) and will take
    up space, but 0 wait-state is possible.
    */
    /*
    IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
    {

    IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)

    }
    */
    /* Uncomment the section below if calling the IQNasin() or IQasin()
    functions from the IQMath.lib library in order to utilize the
    relevant IQ Math table in Boot ROM (This saves space and Boot ROM
    is 1 wait-state). If this section is not uncommented, IQmathTables2
    will be loaded into other memory (SARAM, Flash, etc.) and will take
    up space, but 0 wait-state is possible.
    */
    /*
    IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
    {

    IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)

    }
    */

    /* .reset is a standard section used by the compiler. It contains the */
    /* the address of the start of _c_int00 for C Code. /*
    /* When using the boot ROM this section and the CPU vector */
    /* table is not needed. Thus the default type is set here to */
    /* DSECT */
    .reset : > RESET, PAGE = 0, TYPE = DSECT
    vectors : > VECTORS PAGE = 0, TYPE = DSECT

    }

    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
  • Please clarify your question. Also, please try running other CLA examples.

    sal
  • Please look for WIKI pages and other E2E forum threads concerning the printf.

    sal