Hi,
I noticed that the MCU on my custom board gets warm during the normal operation. I'm using 2 PWM output signal, two input ADC channels, two LEDs and CAN communications. The MCU is warm even if I don't have any output but two blinking LEDs. Is there anyway to run the MCU cooler? Can I decrease the frequency clock and/or disable the other ADC channels to run it more efficiently?
Thanks,