Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE
Hello,
First of all, my apologies if this is not the right place to post this.
Im using a linux based board that has the microcontroller mentioned on this question. I have a temperature-humidity sensor, more specifically this one "DHT22" , that i would like to connect to my board and make reading through GPIO. Im quite new on this GPIO programing and all I found are libs for Rpi or arduino which have different controllers than this. SO i was wondering if it's possible to gt some code sample that would help me a bit on this matter or may be somebody already implemented this and can give me a short explanation on how to do it.
Regards
PD: I would like to make it on c/c++