Part Number: TMS320F28335
Hi, I am using a control platform based on TMS320F28335. I have a setup with a limited no. of output pins. So, I tried to enable only ePWM 5A and not enable ePWM 5B. Is this even possible to do? If it is possible, I intend to use GPIO 9 (which is used in ePWM 5B) as a regular GPIO. Can someone confirm?