Part Number: TMS320F28069
Tool/software: Code Composer Studio
Hi,
I am using TMS320F28069 microcontroller with 14 pin JTAG emulator. Recently when I try to debug, I am getting this error.
C28xx: Error: (Error -1156 @ 0x0) Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device. (Emulation package 6.0.628.1)
If I choose yes, it says,
C28xx: Trouble Halting Target CPU: (Error -2062 @ 0x0) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.1)
But if I run the some example program from the resource explorer, it works fine. Can someone please explain me what to do.
Thanks,
Ponnarasi.