This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-F28377S: F28377s CAN setup problems

Part Number: LAUNCHXL-F28377S

Tool/software: Code Composer Studio

I can send CAN messages fine, but I cannot receive anything.

Setup:

LaunchXL_F28377s with a PCAN explorer dongle (running PCAN explorer 5 on the PC).  I've also tested this with other CAN devices without issue.  I've got a working version on the F28069 Launch Pad, but the CAN drivers here are so different, they can't be used, but the hardware setup shows it's working just fine..

Program: I tried my own and had issues, so I'm working straight off of the can_external_transmit_cpu1 example project for the 28377s

Compiler: 17.6.0.STS

I've modified to program to only use CAN A (also to properly set the clock which is not correct for the launchpad initially). 

//GPIO init:

GPIO_SetupPinMux(70, GPIO_MUX_CPU1, 5); //GPIO30 - CANRXA

GPIO_SetupPinOptions(70, GPIO_INPUT, GPIO_ASYNC);


GPIO_SetupPinMux(71, GPIO_MUX_CPU1, 5); //GPIO31 - CANTXA
GPIO_SetupPinOptions(71, GPIO_OUTPUT, GPIO_PUSHPULL);

What works:

I can transmit just fine, although it does trigger an interrupt on a successful transmit even though this is not requested (I've triple checked this).

What doesn't work:

I can receive a CAN message and that triggers an interrupt,  but when trying to read the message back the PID is always 0, the length is always 0, and the data doesn't appear to come in as well.

I've tried changing the MsGID on the RxMessage Template to zero.  I've tried matching it to what I'm sending.  I've tried extended and standard frames.  Nothing but zeros always...

Also note, when trying to read CanaRegs via the expressions window, it comes back with an Error: "Memory map prevented reading 0x00048080@Data"  

Any help would be appreciated.

Thanks!

Source code of the program (modified TI example) is below:

//###########################################################################
//
// FILE:   can_external_transmit.c
//
// TITLE:  Example to demonstrate CAN external transmission
//
//! \addtogroup cpu01_example_list
//! <h1>CAN-A to CAN-B External Transmit (can_external_transmit)</h1>
//!
//! This example initializes CAN module A and CAN module B for external
//! communication. CAN-A module is setup to transmit incrementing data for "n"
//! number of times to the CAN-B module, where "n" is the value of TXCOUNT.
//! CAN-B module is setup to trigger an interrupt service routine (ISR) when
//! data is received. An error flag will be set if the transmitted data doesn't
//! match the received data.
//!
//! \note Both CAN modules on the device need to be
//!       connected to each other via CAN transceivers.
//!
//! \b External \b Connections \n
//!  - CANA is on GPIO31 (CANTXA) and GPIO30 (CANRXA)
//!  - CANB is on GPIO8 (CANTXB) and GPIO10 (CANRXB)
//!
//! \b Watch \b Variables \n
//!  - TXCOUNT - Adjust to set the number of messages to be transmitted
//!  - txMsgCount - A counter for the number of messages sent
//!  - rxMsgCount - A counter for the number of messages received
//!  - txMsgData - An array with the data being sent
//!  - rxMsgData - An array with the data that was received
//!  - errorFlag - A flag that indicates an error has occurred
//!
//
//###########################################################################
// $TI Release: F2837xS Support Library v3.01.00.00 $
// $Release Date: Mon May 22 15:44:59 CDT 2017 $
// $Copyright:
// Copyright (C) 2014-2017 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without 
// modification, are permitted provided that the following conditions 
// are met:
// 
//   Redistributions of source code must retain the above copyright 
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the 
//   documentation and/or other materials provided with the   
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################

//
// Included Files
//
#include "F28x_Project.h"     // Device Headerfile and Examples Include File
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "inc/hw_can.h"
#include "driverlib/can.h"

//
// Defines
//
#define TXCOUNT  100
#define MSG_DATA_LENGTH    8
#define TX_MSG_OBJ_ID    15
#define RX_MSG_OBJ_ID    1

//
// Globals
//
volatile unsigned long i;
volatile uint32_t txMsgCount = 0;
volatile uint32_t rxMsgCount = 0;
volatile uint32_t errorFlag = 0;
unsigned char txMsgData[4];
unsigned char rxMsgData[4];
tCANMsgObject sTXCANMessage;
tCANMsgObject sRXCANMessage;

//
// Function Prototypes
//
__interrupt void canaISR(void);

//
// Main
//
void main(void)
{
    //
    // Initialize System Control:
    // PLL, WatchDog, enable Peripheral Clocks
    //
    InitSysCtrl();

    //
    // Initialize GPIO and configure GPIO pins for CANTX/CANRX
    // on module A and B
    //
    InitGpio();

    //
    // Setup GPIO pin mux for CAN-A TX/RX and CAN-B TX/RX
    //
    GPIO_SetupPinMux(70, GPIO_MUX_CPU1, 5); //GPIO30 -  CANRXA
    GPIO_SetupPinOptions(70, GPIO_INPUT, GPIO_ASYNC);
    GPIO_SetupPinMux(71, GPIO_MUX_CPU1, 5); //GPIO31 - CANTXA
    GPIO_SetupPinOptions(71, GPIO_OUTPUT, GPIO_PUSHPULL);
    /*
    GPIO_SetupPinMux(10, GPIO_MUX_CPU1, 2); //GPIO10 -  CANRXB
    GPIO_SetupPinOptions(10, GPIO_INPUT, GPIO_ASYNC);
    GPIO_SetupPinMux(8, GPIO_MUX_CPU1, 2);  //GPIO8 - CANTXB
    GPIO_SetupPinOptions(8, GPIO_OUTPUT, GPIO_PUSHPULL);
    */
    //
    // Initialize the CAN controllers
    //
    CANInit(CANA_BASE);
    //CANInit(CANB_BASE);

    //
    // Setup CAN to be clocked off the PLL output clock
    //
    CANClkSourceSelect(CANA_BASE, 0);   // 500kHz CAN-Clock
    //CANClkSourceSelect(CANB_BASE, 0);   // 500kHz CAN-Clock

    //
    // Set up the CAN bus bit rate to 500kHz for each module
    // This function sets up the CAN bus timing for a nominal configuration.
    // You can achieve more control over the CAN bus timing by using the
    // function CANBitTimingSet() instead of this one, if needed.
    // Additionally, consult the device data sheet for more information about
    // the CAN module clocking.
    //
    CANBitRateSet(CANA_BASE, 200000000, 250000);
    //CANBitRateSet(CANB_BASE, 200000000, 500000);

    //
    // Enable interrupts on the CAN B peripheral.
    //
    CANIntEnable(CANA_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);

    //
    // Clear all interrupts and initialize PIE vector table:
    // Disable CPU interrupts
    //
    DINT;

    //
    // Initialize the PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    //
    InitPieCtrl();

    //
    // Disable CPU interrupts and clear all CPU interrupt flags
    //
    IER = 0x0000;
    IFR = 0x0000;

    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example.  This is useful for debug purposes.
    //
    InitPieVectTable();

    //
    // Interrupts that are used in this example are re-mapped to
    // ISR functions found within this file.
    // This registers the interrupt handler in PIE vector table.
    //
    EALLOW;
    PieVectTable.CANA0_INT = canaISR;
    EDIS;

    //
    // Enable the CAN-B interrupt on the processor (PIE).
    //
    PieCtrlRegs.PIEIER9.bit.INTx5 = 1;
    IER |= M_INT9;
    EINT;

    //
    // Enable the CAN-B interrupt signal
    //
    CANGlobalIntEnable(CANA_BASE, CAN_GLB_INT_CANINT0);

    //
    // Initialize the transmit message object used for sending CAN messages.
    // Message Object Parameters:
    //      Message Identifier: 0x5555
    //      Message ID Mask: 0x0
    //      Message Object Flags: None
    //      Message Data Length: 4 Bytes
    //      Message Transmit data: txMsgData
    //
    sTXCANMessage.ui32MsgID = 0x5555;
    sTXCANMessage.ui32MsgIDMask = 0;
    sTXCANMessage.ui32Flags = 0;
    sTXCANMessage.ui32MsgLen = MSG_DATA_LENGTH;
    sTXCANMessage.pucMsgData = txMsgData;

    //
    // Initialize the receive message object used for receiving CAN messages.
    // Message Object Parameters:
    //      Message Identifier: 0x5555
    //      Message ID Mask: 0x0
    //      Message Object Flags: Receive Interrupt
    //      Message Data Length: 4 Bytes
    //      Message Receive data: rxMsgData
    //
    sRXCANMessage.ui32MsgID = 0x0;
    sRXCANMessage.ui32MsgIDMask = 0;
    sRXCANMessage.ui32Flags = MSG_OBJ_RX_INT_ENABLE;
    sRXCANMessage.ui32MsgLen = MSG_DATA_LENGTH;
    sRXCANMessage.pucMsgData = rxMsgData;
    CANMessageSet(CANA_BASE, RX_MSG_OBJ_ID, &sRXCANMessage,
                  MSG_OBJ_TYPE_RX);

    //
    // Initialize the transmit message object data buffer to be sent
    //
    txMsgData[0] = 0x12;
    txMsgData[1] = 0x34;
    txMsgData[2] = 0x56;
    txMsgData[3] = 0x78;

    //
    // Start CAN module A and B operations
    //
    CANEnable(CANA_BASE);
    //CANEnable(CANB_BASE);

    //
    // Transmit messages from CAN-A to CAN-B
    //
    while(1)
    {
        //
        // Check the error flag to see if errors occurred
        //
        if(errorFlag)
        {
            //asm("   ESTOP0");
        }

        //
        // Verify that the number of transmitted messages equal the number of
        // messages received before sending a new message
        //
        //
        // Transmit Message
        //
        //CANMessageSet(CANA_BASE, TX_MSG_OBJ_ID, &sTXCANMessage, MSG_OBJ_TYPE_TX);

        //txMsgCount++;


        //
        // Delay 0.25 second before continuing
        //
        DELAY_US(1000 * 250);

        //
        // Increment the value in the transmitted message data.
        //
        txMsgData[0] += 0x01;
        txMsgData[1] += 0x01;
        txMsgData[2] += 0x01;
        txMsgData[3] += 0x01;
        
        //
        // Reset data if exceeds a byte
        //
        if(txMsgData[0] > 0xFF)
        {
            txMsgData[0] = 0;  
        }
        if(txMsgData[1] > 0xFF)
        {
            txMsgData[1] = 0; 
        }     
        if(txMsgData[2] > 0xFF)
        {
            txMsgData[2] = 0; 
        }     
        if(txMsgData[3] > 0xFF)
        {
            txMsgData[3] = 0; 
        }         
    }

    //
    // Stop application
    //
    asm("   ESTOP0");
}

//
// CAN B ISR - The interrupt service routine called when a CAN interrupt is
//             triggered on CAN module B.
//
__interrupt void canaISR(void)
{
    uint32_t status;

    //
    // Read the CAN-B interrupt status to find the cause of the interrupt
    //
    status = CANIntStatus(CANA_BASE, CAN_INT_STS_CAUSE);

    //
    // If the cause is a controller status interrupt, then get the status
    //
    if(status == CAN_INT_INT0ID_STATUS)
    {
        //
        // Read the controller status.  This will return a field of status
        // error bits that can indicate various errors.  Error processing
        // is not done in this example for simplicity.  Refer to the
        // API documentation for details about the error status bits.
        // The act of reading this status will clear the interrupt.
        //
        status = CANStatusGet(CANA_BASE, CAN_STS_CONTROL);

        //
        // Check to see if an error occurred.
        //
        if(((status  & ~(CAN_ES_RXOK)) != 7) &&
           ((status  & ~(CAN_ES_RXOK)) != 0))
        {
            //
            // Set a flag to indicate some errors may have occurred.
            //
            errorFlag = 1;
        }else
        {
            CANMessageGet(CANA_BASE, RX_MSG_OBJ_ID, &sRXCANMessage, true);

            //
            // Getting to this point means that the RX interrupt occurred on
            // message object 1, and the message RX is complete.  Clear the
            // message object interrupt.
            //
            CANIntClear(CANA_BASE, RX_MSG_OBJ_ID);
        }
    }
    //
    // Check if the cause is the CAN-B receive message object 1
    //
    else if(status == RX_MSG_OBJ_ID)
    {
        //
        // Get the received message
        //
        CANMessageGet(CANA_BASE, RX_MSG_OBJ_ID, &sRXCANMessage, true);

        //
        // Getting to this point means that the RX interrupt occurred on
        // message object 1, and the message RX is complete.  Clear the
        // message object interrupt.
        //
        CANIntClear(CANA_BASE, RX_MSG_OBJ_ID);

        //
        // Increment a counter to keep track of how many messages have been
        // received. In a real application this could be used to set flags to
        // indicate when a message is received.
        //
        rxMsgCount++;

        //
        // Since the message was received, clear any error flags.
        //
        errorFlag = 0;
    }
    //
    // If something unexpected caused the interrupt, this would handle it.
    //
    else
    {
        //
        // Spurious interrupt handling can go here.
        //
    }

    //
    // Clear the global interrupt flag for the CAN interrupt line
    //
    CANGlobalIntClear(CANA_BASE, CAN_GLB_INT_CANINT0);

    //
    // Acknowledge this interrupt located in group 9
    //
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP9;
}

//
// End of File
//

  • Hello,
    I am writing to let you know that a C2000 team member has been assigned to this post and should be answering shortly.

    Regards
    Baskaran
  • I've traced it to how the functions setup the Acceptance mask.

    I've traced it down to the actual registers where IF1MSK are being written as 0x20000000 and IF1ARB is written as 0x80000000, which according to the datasheet is correct for "Accept all messages"...  so that seems correct.

    However the CANMessageSet(...) function doesn't set IF1CMD Mask to actually write these values to the message RAM unless the flag  "MSG_OBJ_USE_ID_FILTER" is set which is counter intuitive.  That doesn't fully fix the issue either.

    CANMessageSet does not Set UMask in IF1MCTL to the use the acceptance mask unless the flag "MSG_OBJ_USE_ID_FILTER"  is set as well.  In general this makes sense, but in reality I can't seem to get any information from the messages unless this bit is set.  

    So, if you want an "Accept all/any"  message you have to set the acceptance filter to 0, and check that you are indeed using the acceptance filter...  This doesn't seem to match what specification sheet says.

    For people looking to use the can.c/can.h in the future, you will want to use this to setup a generic mailbox:

    sRXCANMessage.ui32MsgID = 0x0;
    sRXCANMessage.ui32MsgIDMask = 0x0;
    sRXCANMessage.ui32Flags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER;
    sRXCANMessage.ui32MsgLen = MSG_DATA_LENGTH;
    sRXCANMessage.pucMsgData = rxMsgData;
    CANMessageSet(CANA_BASE, RX_MSG_OBJ_ID, &sRXCANMessage, MSG_OBJ_TYPE_RX);

    Thanks,

    Kyle M