This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI C/C++ Compiler
I use the controlsuit example "blinky_cpu01" of 28377D .
when I config the sysclk ," InitSysPll(XTAL_OSC, IMULT_20, FMULT_0, PLLCLK_BY_2);" The CCS will prompt error:
C28xx_CPU1: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 5.1.641.0)
C28xx_CPU1: Unable to determine target status after 20 attempts
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
but when I config the sysclk ," InitSysPll(XTAL_OSC, IMULT_3, FMULT_0, PLLCLK_BY_2);" It will generate 30MHz CLK, the program will run normally. and the LED will blinky slowly.
I want to know why I cannot config the CLK normally.
Hi,
It looks like current starvation issue, when you try to lock the PLL at 200MHz and use that as SYSCLK, there will be surge in current that need to be supported by the VDD core supply as per the data sheet spec (IDD max = 440mA).
Did you make sure your supply is clean and supports 440mA of current?
If you increase the speed gradually i.e. IMULT = 3, 6, 10, 12, 15, 18, 20; do you see the PLL lock without getting any error?
Regards,
Nirav