This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28377S: Sine output on buffered dac example program

Part Number: LAUNCHXL-F28377S

Hello

i  just got launch pad and i tried running the buffered dac sine example and i got confused at which pin i should probe
on the pin diagram i got with the unit there are dac1, dac2, dac3, dac4, while on the user guide there is daca, dacb, dacc, dacd

while runing in debugging  mode i can see there are values in daca registeres, and i tried scoping all of the four dacs from 1 do 4 and i get 0v at all the outputs

am i probing the wrong pins or is there something else im doing wrong here?