Part Number: F28M35H52C
Other Parts Discussed in Thread: CONTROLSUITE
I'm using the F28M35H52C1 Concerto on a custom board
I'm trying to configure ePWM7 on the C28 core but all the registers remain 0 after i run my initialize code.
ePWM1 is functional
My first guess that the registers are not being clock... ?? but I haven't found anything yet.
Any ideas where to check?
thanks
Greg
Code below:
M3:
SysCtlClockConfigSet(SYSCTL_USE_PLL | (SYSCTL_SPLLIMULT_M & 0xF) | SYSCTL_SYSDIV_1 | SYSCTL_M3SSDIV_2 | SYSCTL_XCLKDIV_4);
C28:
Note: period is calculated else where before hand
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; // Stop all the TB clocks
EDIS;
// ------------------------------------------------------------------------
// EPWM1 - Master
EPwm1Regs.TBPRD = period; // Time-Base Period, PWM frequency = 1 / period
EPwm1Regs.TBPHS.all = 0; // Time-Base Phase
EPwm1Regs.TBCTR = 0; // Time-Base Counter
// Time-Base Clocks
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count Up-Down mode: used for symmetric PWM
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Master module
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; // Sync down-stream module
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW; // Set load from Shadow register
// Interrupts
EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_PRD;
EPwm1Regs.ETSEL.bit.INTEN = 1; // Enable INT
EPwm1Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on every event
// ------------------------------------------------------------------------
// EPWM7
EPwm7Regs.TBPRD = period; // Time-Base Period
EPwm7Regs.TBPHS.all = 0; // Time-Base Phase
EPwm7Regs.TBCTR = 0; // Time-Base Counter
// Time-Base Clocks
EPwm7Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count-updown mode: used for symmetric PWM
EPwm7Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Slave to EPWM1
EPwm7Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm7Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm7Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
EPwm7Regs.TBCTL.bit.PRDLD = TB_SHADOW; // Set Immediate load
// Setup shadow register load on ZERO
EPwm7Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm7Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm7Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR=Zero
EPwm7Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR=Zero
// Set Compare values
EPwm7Regs.CMPA.half.CMPA = period+1; // Set A LOW initially
EPwm7Regs.CMPB = 0; // Set B HIGH initially
// Set actions
EPwm7Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM7A on event A, up count
EPwm7Regs.AQCTLA.bit.CAD = AQ_CLEAR; // Clear PWM7A on event A, down count
EPwm7Regs.AQCTLB.bit.CBU = AQ_SET; // Set PWM7B on event B, up count
EPwm7Regs.AQCTLB.bit.CBD = AQ_CLEAR; // Clear PWM7B on event B, down count
// DeadBand configuration
EPwm7Regs.DBCTL.bit.IN_MODE = DBA_ALL; // EPWM7A is the source for both falling-edge and rising-edge delay
EPwm7Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; // Both the falling-edge delay (FED) and rising-edge delay (RED) are applied to the input signals
//EPwm7Regs.DBCTL.bit.OUT_MODE = DB_DISABLE;
EPwm7Regs.DBCTL.bit.POLSEL = DB_ACTV_HI; // Active High
EPwm7Regs.DBRED = RED_DELAY_B; // Set DeadBand time for rising edge
EPwm7Regs.DBFED = FED_DELAY_B; // Set DeadBand time for falling edge