This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help in selecting a processor for logging digital bits every 5 us

I have designed a circuit board which based on input signal pulse,generates 40 bits containing pulse width, peak and time of arrival of the pulse

Specifically I need a controller/processor which can read and store these 40 bits to a memory every 5 us. It should also support USB interface, so that I can transfer the data to a computer,  and it doesn't fill the onboard flash.

Could you please help suggest a controller pertaining to this task?

Thanks,

Ashutosh