Part Number: TMS320F28069M
Tool/software: TI C/C++ Compiler
Hello,
I am trying to add my own .cio section to the memory. Looking into the linker command file, I can see that:
a) some memory ranges overlap nicely, ex:
BEGIN: origin (0x50) + length (0x02) = BOOT_RSVD: origin (0x02) BOOT_RSVD: origin (0x02) + length (0x4E) = RAMM0: origin (0x50) RAMM0: origin (0x50) + length (0x3B0) = RAMM1: origin (0x400)
...and so on.
b) BUT there are a few memory ranges that seem to leave some unused space. Ex:
RAMM1: origin (0x400) + length (0x400) = 0x800
and the next section starts from 0x8000:
RAML0_L8 : origin = 0x008000,
(1) Does it mean that I can safely increase RAMM1 length to 7C00?
I have actually tried that (even with a smaller value to keep some margin) and then assigned .cio section to RAMM1. The result? I get following console message when running the program (probably connected to printf function):
"Invalid CIO command (0) in the CIO buffer at address (0x800) was not recognized. Please check the device and program memory maps."
The map file says that .cio was assigned specifically to 0x800.
(2) Can it be that there is some memory overlap at 0x800 after I increased the size of RAMM1 over this default limit? I cannot see any other section at this value!
Another question is:
(3) What is the best memory range to allocate .cio section to? By default (if not implemented in the linker file) it is placed in USB_RAM. Is it OK to use the same range?