Part Number: TMS320F280049M
Hi Champs,
My one of customer is evaluating CAN with F280049M. They configured the CAN massage object as following code to receive mixed CAN Identifiers on same CAN node. Some message objects are configured with Standard ID and anothers are set with Extended ID.
In this case, CAN module seems do not work properly. If they do not configure message objects that is configured as Standard Id, the message objects that has Extended Id work well. It also works well in the other way.
Can F28004x configure a mixed CAN Identifier? If so what's wrong on the following configuration code for CAN message object?
Regards