This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSHVMTRPFCKIT: Hardware requirements for e-scooter controller

Part Number: TMDSHVMTRPFCKIT


We are planning to build a controller for e-scooter using Piccolo F28035. We have gone through the following application report, http://www.ti.com/lit/an/slva642/slva642.pdf

  • Hi Reshma,
    Do you have any specific questions over what is described in the pdf. I suppose the HW requirements are listed in the doc itself.

    Regards
    Baskaran
  • Hi,

    Thank you for your reply.

    The doc contains a section titled "Hardware Blocks" which describes all the hardware requirements.But we need to know whether all the components listed under the "Hardware Blocks" are integrated in the kit. Or what are the additional hardware requirements? We own only this kit and an  AVON e-scooter (E scoot 207). 

  • Which EVM kit do you want to refer?
    This document you linked is a application notes which introduce how to design a hardware circuit for a E-bike, don't have a related EVM kit. The required modules based on your design specification, a general motor drive board must have controller, power supply, current/voltage sensing, over current/voltage protection and power inverter modules. You need to know what input voltage, rated output power, rated speed, maximum current of motor, and then to design your hardware board.