Part Number: F28M36H53C2
Other Parts Discussed in Thread: CONTROLSUITE
Hello,
I hope that anybody can give me some quick advice from where to start my development.
I would like pilot my ePWMs based on the value of the output of and ADC. I had a bit of study on that and if my understand is correct I should put in place something using a combination of the analog comparator; the digital compartor and the trip zone in the ePWM module.
Now as far as I understood the GPIO pin of interest for this should be the one associated to GPIMUX2, namely GPIO193-GPIO197 + GPIO199.
But I don't understand if it is possible to use internally link some ADC output to this GPIO pins?
I am sure I am missing something any suggestion on this topic would be really appreciated.
Claudio