Part Number: TMS320F28069M
Other Parts Discussed in Thread: TMS320F28069
Hi,
I have two TMS320F28069 MCUs that I'm not able to program on my custom boards. When I power up the board, the reset pin on the MCU becomes low while I connect it to 3.3V through a resistor. I can read 0 volt on this pin but when I remove the MCU from the board, I can read 3.3 after the resistor. This means that the reset pin got pulled down through the MCU. Does this mean the MCU is broken? because it should be a pull up channel. :(