Other Parts Discussed in Thread: CONTROLSUITE
Are interrupts preemptive? For example, if I'm in dispatched HWI function, can I assume that no other HWIs or ISRs will interrupt the first function?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CONTROLSUITE
Are interrupts preemptive? For example, if I'm in dispatched HWI function, can I assume that no other HWIs or ISRs will interrupt the first function?
In an ISR, software can enable only the interrupts that it would like to interrupt that ISR, and then re-enable the global interrupt mask. There is an example in the peripheral header files of a full-blown prioritization scheme. Most users just want to nest one or two interrupts though, so it is easily handled with a few lines of code.
if you have www.ti.com/controlsuite installed
C:\ti\controlSUITE\device_support\f2803x\v122\DSP2803x_examples_ccsv4\sw_prioritized_interrupts
here is the INT section of the Piccolo 1-day Workshop
http://processors.wiki.ti.com/index.php/C2000_Piccolo_One-Day_Workshop_Module_2#Interrupts
3-day workshop has more details
http://processors.wiki.ti.com/index.php/C2000_Piccolo_Multi-Day_Workshop
Chapter 6 of the Teaching ROM is also excellent (and there are examples for all C2000 families)
http://www.ti.com/ww/eu/university/roms.html
So the default behavior is that new interrupts would NOT preempt an ISR in progress? Including dispatched HWI in DSP-BIOS?