Part Number: LAUNCHXL-F28379D
Hi Great Team ,
I have to plug a 20 pin connector IDC on the J5 /J7, but it is impossible for the thick jumper on JP5 and JP4 (they are too thick) . If I remove both jumper I can insert the 20 PIN connector IDC on the J5/J7.
My question is: "If I remove both jumper there may be problems? My software will work the same way as when the two jumper are inserted? (My software use 8PWM module, 4ADC module, 2SPI module, PIN 3.3V and PIN GND of J1/J3 and J5/J7 to supply two external modules).
JP5 and JP4 are respectively "Connects target MCU 3.3 V to second set of BoosterPack headers" and "Connects target MCU 5 V to second set of BoosterPack headers".
Thanks