Part Number: TMS320F28379D
Tool/software: Code Composer Studio
Hi,
I am trying to get two DSPs work together and what I did is to use some GPIOs to sync two DSPs. I directly connect GPIOs on one DSP to another, setting them as output/input of 1st/2nd DSP. The problem is, sometimes I lost the synchronization between two DSPs but sometimes they can be synced very well. My question is:
1. Is it ok to directly connect the output GPIO of DSP#1 to the input GPIO of DSP#2?
2. Does EPWM_ISR have strict timing? Will there be something wrong occasionally?
3. To realize 0-100% duty cycle, is it better to set CMPA/B=PRD/ZRO, or use set/clear function in AQ submodule?
Thanks a lot!!