Part Number: DRV8301-69M-KIT
Other Parts Discussed in Thread: DRV8301
We are trying to build a position based control system based on DRV8301-69M & instaspin FOC & Motion Lab experiments.
We are using Leadshine BLDC motor & are able to run our BLDC motor with GUI composer. The same is not happening with Lab experiment 1b. We are also not able to see the graph output as explained in Lab 1b. When probed, we found that code is waiting for the variable gMotorVars.FlagEnableSys to be set. We could not understand where it is set.
We have also tried changing the motor parameters in user.h (values taken from GUI composer), but no result. We have also tried other lab experiments from 1b onwards. None of them are working for us.
CCS Version 7.2.0 used.
Regards