Other Parts Discussed in Thread: TMS320C28346
Hello, I want to start my program form an externel flash, and I choose Parallel XINTF boot mode for my design, so that my program can be load to internel memory from XD[15:0] when prower up. But it is not the same as I expect. when I set the XA15~XA12 to "0101", and connected GPIO12 to GPIO13 in FPGA, then power up. I found there is a pluse from high to low on signal XZCS6 and XRD, then the two signals held the state of low forever, and the address bus always keep "00000", the data bus had a word "10AA". My clock for TMS320C28346 is 20M. I attach my picture about these phenomemons, please help me to slove this problem.