Part Number: TMS320F28035
Other Parts Discussed in Thread: TMS320F28069, TMS320F28065, TMS320F280049
Hi team,
I'm currently working with TMS320F28035 and am running out of RAM. I'm looking for an alternative with the following requirements...
| SYS CLK | >= 60MHz |
| RAM | >= 56KB |
| Flash | >= 128KB |
| CLA | Yes |
| FPU | Yes |
| GPIO | 34 |
| PWM Channels (A,B) | 6 |
| I2C | 1 |
| SCI | 2 |
| Timer | 3 |
| Watchdog | 1 |
| ADC Channels | 12 |
It looks like TMS320F28069 is a good match--is there anything else you would recommend, or is this the best option?
Thanks,
Brian Angiel