This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377D: Load program Error: .out: a data verification error occurred file load failed.

Part Number: TMS320F28377D


Tool/software: Code Composer Studio

I use CCS6.1 and controlsuit example. At first, I use RAM to debug, and everything is OK, Now, I use FLSAH to debug, I can build the project success, and the '.ccxml' shows that  target can connect the DSP. But I can't load .out and debug the project. please help me.Thank you.

C28xx_cpu1:verification failed:value at address 0x82000 do not match Please verify target memory and memory map.