This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28377S: FPU, execution time

Part Number: TMS320F28377S


Tool/software: TI C/C++ Compiler

Hi to all,

In my project I use FPU library to calculate a fir filter ( order 1023) on signal acquired from ADC and put the result on DAC.

In my test I would to measure the execution time of

hnd_firFP->calc(&firFP);

to do that I put a gipo High prior to call the calc function, and return to low state after the calc function, and use an oscilloscope to monitor the pin activity.

What I see is that the calc function take aboute 5,6 us but often it take about 10us.

How do you explain this beaviours?

I thought htat is a problem of variable allign, so I modify the linker command adding 3 line:

  firldb    ALIGN(0x800)	 > RAMGS10,PAGE = 1, fill=0x0400
  coefffilt ALIGN(0x800)	 > RAMGS11,PAGE = 1, fill=0x0400
  firfilt   				 > RAMLS5 ,PAGE = 1, fill=0x0100

But the problem is still here. It's correct my change in linker ommand?

Thanks!

  • Antonino,

    F28377S CPU clock is 200MHz, i.e. 5nS for 1023 order filter, 5x(1023+52)=5.375uS makes sense

    Make sure you have disabled any interrupts that are a higher priority before you begin profiling.

    If you have additional higher priority interrupts the code may branch to those and thus affecting the apparent delay you observe