Part Number: DRV8301-69m-kit
Other Parts Discussed in Thread: MOTORWARE
Tool/software: TI C/C++ Compiler
I am getting ERROR #10234-D : when building Lab12b.c with throttle control.
I have no problem when using same device (throttle) with Lab3a.c .
Originally, I experienced problems (errors on Lab3a.c ) using HAL INSTUCTION.
But after implementing Oscar D Molina DRV 8301 with bike throttle (FORUM) solution on
Global Variables , the errors on Lab3a.c got resolved and w as able to use the Throttle control.
Now I am using the same with Lab12b but having these problems:
"C:/ti/motorware/motorware_1_01_00_17/sw/ide/ccs/cmd/f2806x/f28069m_ram_lnk.cmd"
<Linking>
undefined first referenced
symbol in file
__________ _____________
_Hal_readPotentiometerData ./proj_lab12b.obj
ERROR #10234-D : unresolved symbols remain
ERROR #10010: errors encountered during linking; "proj_lab12b.out" not built
>> Compilation failure
makefile:167 recipe for target 'proj_lab12b.out' failed
gmake: *** [proj_lab12b.out] Error 1
gmake: Target 'all' not remade because of errors.
**** Build Finished ****
Thank you for your support .
roy