Hi all,
what kind of problems will occur when change from analog PI control to digital PI control?
Here is my situation:
1.I have recently using the analog PI control to control the current, the analog PI output is sampled via the ADC inside f2808 and the result is very satisfying, current ripple only 0.7A out of 10A
2.Based on the analog control scheme, I used the digital PI controller from TI and the current ripple increases to 1.4A out of 10A
3.I reduced the system's bandwidth trying to bring the current ripple down but without success
3.Since the current ripple limitation has to be below 1A, can anyone share your experience when using digital PI control before? Will the performance really be reduced when changed to digital control?
Thanks!
Bill