Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
I have tested my program in RAM and now I am ready to convert to Flash. I am using Code Composer Studio version 6.2
I opened the Properties for my project, in the General section I am browsing the "Linker command file:" in D:\ti\ccs620\ccsv6\ccs_base\c2000\include.
I do not see a file for the F28377D. I see F28335.cmd, & 28377S_FLASH_lnk.cmd, & 2837x_FLASH_lnk_cpu1.cmd.
I chose 2837x_FLASH_lnk_cpu1.cmd, but when I compile I get the following errors.
warning #10247-D: creating output section "ramfuncs" without a SECTIONS
warning #10247-D: creating output section "TrigRegsFile" without a SECTIONS
warning #10247-D: creating output section "IpcRegsFile" without a SECTIONS